Feedback_Kv
| Index.Sub | 2230.05H |
| Data Type | Unsigned32 |
| Access | Read/Write |
| PDO Mappable | No |
| Unit |
-- |
|
Range |
Unsigned32 |
| Default Value |
8000 |
| Store Supported | Yes |
| Description | This value is used for Closed Loop feature and defines the velocity gain of PID’s regulator. The value has to be adjust to keep the velocity error (Feedback_Actual_Velocity_Error) inside the tolerance of application. |
|
Notes |
A value too high could introduce motor’s vibration. |